The following communication objects are used to control the "Solar protection control” function:
A + B Solar Protection
A Solar Protection
No. | Object name | Function | Datapoint type | Flags |
---|---|---|---|---|
10 | A + B Solar Protection A Solar Protection | Up/Down | 1.008 up/down | CRWT |
Function:
The telegrams “solar protection up” or “solar protection down” are sent via the group address linked with this communication object.
Availability: Communication object “A + B Solar Protection”
The "A + B Solar Protection” communication object is displayed if the following configurations have been made:
- Parameter "Function channels A + B” on the "device settings” parameter card
- Setting: “Single”
- Parameter "Function channel” on the “functions, objects” parameter card
- Setting: “Solar protection control”
Availability: Communication object “A Solar Protection”
The "A Solar Protection” communication object is displayed if the following configurations have been made:
- Parameter "Function channels A + B” on the "device settings” parameter card
- Setting: “Pairwise”
- Parameter "Function channels” on the “functions, objects” parameter card
- Setting: “Solar protection control”
More information:
A + B Slats
A Slats
No. | Object name | Function | Datapoint type | Flags |
---|---|---|---|---|
11 | A + B Slats A Slats | Stop, Up/Down | 1.007 step | CRT |
Function:
The telegrams “slats open,” “slats closed” or “stop” are sent via the group address linked with this communication object. If the solar protection is in motion, the “stop” telegram is sent. In the solar protection is not moving, the last stored direction in which the slats moved is inverted and the opposite telegram is sent.
Availability: Communication object “A + B Slats”
The "A + B Slats” communication object is displayed if the following configurations have been made:
- Parameter "Function channels A + B” on the "device settings” parameter card
- Setting: “Single”
- Parameter "Function channel” on the “functions, objects” parameter card
- Setting: “Solar protection control”
Availability: Communication object “A Slats”
The "A Slats” communication object is displayed if the following configurations have been made:
- Parameter "Function channels A + B” on the "device settings” parameter card
- Setting: “Pairwise”
- Parameter "Function channels” on the “functions, objects” parameter card
- Setting: “Solar protection control”
More information: