Enabling and customizing email messages - Online Help

Building X Workplace Experience Online Help

Product Family
Building X
Content Language
English
Content Type
Technical Documentation > Online Help
Document No
A6V15295253_en--
Download ID
A6V15295253
Access level
Internet
File Type
html

Features

  • All messages are disabled by default.
  • The email content is pre-set but can be customized.
  • The booking data elements are prefixed with a hash (i.e., #_desk_name), which should not be altered. Other text can be modified as needed.
  • Desk check-in and auto-release email timing is controlled from the Occupancy and Auto-Release Settings.

Info

Messages for Auto-release require Occupancy sensors and configuration.

To enable and configure the messages for a building:

  1. Go to Advanced Console > Config.
  2. Select the Building, then select the Go [Arrow] button.
  3. On the Building Config page, scroll down to the Desk booking: Email Reminder Configuration section.
  4. Expand the section for the email message you want to configure.
  5. Check the box to enable the email type.
  6. Desk check-in and auto-release emails show details about the send timing. This info is automatically populated by the relevant threshold parameters set in the Occupancy and Auto-Release Settings. To modify the timing, make changes there.
  7. The email Subject is pre-set but can be customized, and dynamic variables added.
  8. The email body Content is pre-set. The booking data elements are preceded by a hash (i.e., #_desk_name). These should remain as is, but other text can be customized as needed.
  9. Select Save when you're finished with each email.
    alt text